PROFINET.USEMODULECFG
Description
This command controls where the drive obtains the telegram configuration. When set to 1 (default), the drive uses the telegram setting from the module configuration in the PROFINET master. When set to 0, the drive uses the telegram setting specified in AXIS#.PROFINET.TELEGRAMID (P922).
Value | Description |
---|---|
0 |
Drive uses the telegram specified from AXIS#.PROFINET.TELEGRAMID (P922) |
1 (default) |
Drive uses telegram configuration from the sub-module configuration in the PROFINET master. |
-
- When this keyword is set to 1 (use PLC configuration), AXIS#.PROFINET.TELEGRAMID and AXIS#.PROFINET.​SUPPTELEGRAMID keywords are set to read only.
For more information, see Telegram Mappings.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-04-05-000 |
General Information
Type | Read/Write |
Units |
N/A |
Range | 0 to 1 |
Default Value | 1 (Use sub-module configuration from PLC) |
Data Type | Integer |
Stored in Non-Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP
Fieldbus Information
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
PROFINET.USEMODULECFG |
5211 |
Unsigned8 |
Read/Write |
- |